SIEMENS
For the trade press
Erlangen, Germany - Friday, October 23, 2009
Siemens brings world’s first 4000 ampere vacuum circuit breaker for frequent-operation applications without forced cooling onto the market
Siemens is meeting the steel industry’s growing demand for every higher performance levels in melting down scrap metal by launching a refined medium-voltage circuit-breaker. As of September 2009, the company offers 3AH4 vacuum circuit-breakers with an operating current of 4000 amperes (A) for the 36-kilovolt voltage level. It is the first vacuum circuit-breaker worldwide for frequent-operation applications up to 120,000 switching cycles capable of handling such a high operating current without forced cooling. The short-circuit breaking current is 40 kiloamperes (kA) at a voltage of up to 40.5 kilovolts (kV). Siemens has developed these circuit-breakers above all for special applications in the steel industry, such as for switching operations on electric arc furnaces.
EmailImage gallery
The 3AH4 vacuum circuit-breaker is the first vacuum circuit-breaker worldwide for frequent-operation applications up to 120,000 switching cycles capable of handling such a high operating current without forced cooling. The short-circuit breaking current is 40 kiloamperes (kA) at a voltage of up to 40.5 kilovolts (kV)
Siemens has developed the new circuit-breaker above all for special applicaions in the steel industry. There, it can be integrated in the Simetal Sivac-X furnace switchgear supplied by Siemens Industry for switching operations on electric arc furnaces. The switchgear is designed to meet the extremely tough demands made by high-performance electric arc furnaces and ensures reliable power input and reliable plant operation. Furthermore, the long maintenance intervals of up to 10,000 switching cycles boost availability and thus reduce operating costs.

Siemens designed the 3AH4-series frequent-operation circuit-breakers for deployment in harsh ambient conditions such as those encountered in the steel industry. These include high temperatures, high levels of air pollution, instable operating currents, frequent short-circuit trips and operating cycles with more than a hundred switching operations per day. The circuit-breakers are therefore designed as robust post insulators equipped with readily accessible vacuum interrupters. The interrupters can therefore be quickly replaced at the end of their service life after approximately 30,000 switching operations without having to replace the entire circuit-breaker.

Because of the special design of the circuit-breaker air can flow freely along the cooling elements. Operation of the circuit-breaker is therefore possible up to 4000 A without forced cooling. The actuator of the 3AH4-series circuit-breaker is designed for up to 120,000 switching cycles over its entire life cycle. The circuit-breakers are thus also suitable for other areas of application calling for high levels of switching frequency – such as motor control in pumped-storage power plants and in the chemical industry.

“We have more than 35 years of experience in vacuum circuit-breakers. That makes us a reliable partner – especially for capital-intensive industrial applications demanding maximized equipment availability,“ said Wolfgang Heuring, CEO of the Medium Voltage Business Unit within the Siemens Energy Sector.
The Siemens Energy Sector is the world’s leading supplier of a complete spectrum of products, services and solutions for the generation, transmission and distribution of power and for the extraction, conversion and transport of oil and gas. In fiscal 2008 (ended September 30), the Energy Sector had revenues of approximately EUR22.6 billion and received new orders totaling approximately EUR33.4 billion and posted a profit of EUR1.4 billion. On September 30, 2008, the Energy Sector had a work force of approximately 83,500. Further information is available at: http://www.siemens.com/energy.

The Siemens Industry Sector (Erlangen, Germany) is the world's leading supplier of production, transportation, building and lighting technologies. With integrated automation technologies as well as comprehensive industry-specific solutions, Siemens increases the productivity, efficiency and flexibility of its customers in the fields of industry and infrastructure. The Sector consists of six Divisions: Building Technologies, Drive Technologies, Industry Automation, Industry Solutions, Mobility and Osram. With around 222,000 employees worldwide Siemens Industry posted in fiscal year 2008 a profit of EUR3.86 billion with revenues totaling EUR38 billion. http://www.siemens.com/industry
Back
For this item:
Reference No.: EPD200910.014
PictureImage gallery
DownloadDownload document
Drucken Print
EmailSend page www.siemens.com/energy. www.siemens.com/industry Electrical Power Solutions
Innovation
Metal
Simetal
Steel Making
Contact:
Dr. Rainer Schulze  Email
Tel.: +49 (9131) 7-44544
Fax: +49 (9131) 7-25074
rainer.schulze@siemens.com
www.siemens.com
 
 
Siemens AG
Siemens AG
Home  |  Topics  |  Products, Solutions & Services  |  News Center  |  Support  |  About us
International
Site Map | Contact Us
Press Releases
Technical Reports
Press Conferences
Press Pictures
Press Contacts
Fairs and Events