Zimpro wet air oxidation system installed in China.
Wet oxidation is the oxidation of soluble or suspended components in an aqueous environment using oxygen as the oxidizing agent. When air is used as the source of oxygen, the process is referred to as wet air oxidation (WAO). The process will oxidize odorous reduced sulfur species such as sulfides and mercaptides. The system will also break down complex organic contaminants, such as phenols, to either carbon dioxide and water, or biodegradable organics.
The two Sinopec projects are the sixth and seventh spent caustic WAO systems installed in China by Siemens Water Technologies.
Sinopec Tianjin Company (TPCC) is a petrochemical complex of oil refining, ethylene, chemical and chemical fiber production. It is located in the District of Tianjin and has 13 oil refining units, eight chemical production units and five chemical fiber units. Annual crude oil handling capability is about 18 million tons. Sinopec Zhenhai Refining & Chemical Company (ZRCC) is the largest base for crude oil processing, for imported crude oil processing and sour crude oil processing, an oil products export base as well as one of the major crude oil distribution bases in China.
Zimpro WAO systems are a component of the Siemens environmental portfolio. In 2008, revenue from products and solutions of Siemens’ environmental portfolio was nearly EUR19 billion, which is equivalent to around a quarter of Siemens’ total revenue, making Siemens the largest provider of environmentally friendly technology.
Further information about solutions for water treatment is available at http://www.siemens.com/water
A photo supplements this press release. Please see:
http://www.industry.siemens.com/data/presse/pics/IIS200910902.jpg