The new pulsed-bed walnut shell filter is a simple design, has a reduced weight and footprint, and a lower cost when multiple filter systems are used, when compared to conventional filtration.
Walnut shell filtration was developed as a more suitable method of filtering free oil and suspended solids in applications where sand filters have traditionally been used. Today, walnut shell filtration is used to treat oil field produced water, refinery wastewater, and other types of wastewater. Due to the reduction in backwash water volume and reduction in weight and footprint, the new pulsed-bed walnut shell filter is ideal for many off-shore oil production applications.
The pulsed-bed walnut shell filter uses a deep bed of 100 percent black walnut shells, which have excellent surface characteristics for coalescing and filtration, plus superior resilience to attrition. The filter’s deep nutshell bed (66 in., 168 cm) offers superior effluent quality, longer filtration runs, and greater throughput efficiency.
The filter uses raw process water and gas or air for backwashing, eliminating the need for moving mechanical equipment or external scouring equipment. The filter operates at up to twice the flux rate of conventional filters in the same application, and can remove more than three times the amount of solids before needing to be cleaned.
During the filtration cycle, dirty process water passes through the filter from top to bottom. As the water passes through the walnut shell media, free oil and suspended solids are removed.
After 24 hours of filtration, the dirty process water is redirected and pulsed into the bottom of the vessel to fluidize the media bed. In addition, air or process gas is added in a proprietary manner to create an airlift pump. The airlift pump lifts the contaminated media to the top of the
vessel where the turbulence of the backwash water and gas separates oil and suspended solids from the walnut shells. The use of air or gas greatly reduces the amount of backwash
water required. The mixture of air or gas and backwash water is separated in an external vessel. One separator vessel can be used for multiple walnut shell filters. Upon completion of the backwash cycle, the flow of dirty process water is again returned to the top of the vessel.
Further information about solutions for water treatment is available at http://www.siemens.com/water
A picture supplements this press release. Please see:
http://www.industry.siemens.com/data/presse/pics/IIS200905709.jpg