The MBR process can be used with a wide range of municipal and industrial wastewater treatment applications, including water reuse, new housing developments, parks and resorts, and turnkey projects
The MemPulse device introduces air and mixed liquor into the bottom of the membrane modules through an “airlift effect.” The air bubbles blend with the mixed liquor and rise up into membrane fibers, providing effective scouring to the membrane surface and refreshing the membrane surface to prevent solids concentration polarization. The two-phase cross-flow reduces scour air energy dramatically.
No moving parts are added to the system, decreasing operation and maintenance costs. Additionally, there are no mixed liquor jet laterals, which reduces installation time. Rather, the MemPulse MBR device provides even distribution of air and mixed liquor to ensure consistent operating conditions for all of the membrane modules.
The MemPulse MBR system will be featured at WEFTEC.08 in Booth # 28077, Hall B.
Further information about solutions for water treatment available at http://www.siemens.com/water
A photo supplements this press release. Please see:
http://www.industry.siemens.com/data/presse/pics/IIS200810359.jpg